NateS (Customer) asked a question.
I am having trouble with the GS-23 2015 drive with GS20-CM-ENETIP option card. When I go to switch the IP address of the device I am able to change the 9.76-9.79 and everything looks fine. But when I go to send a command to the drive, it throws an error. If I power the drive down for more that a few minutes, it reverts to its original 192.168.1.10 address and I am able to point to that address and communicate with the device just fine. I have no idea why it does not like the address change. I have also tried this on 3 of the exact same drives with the same results.
Looking at the manual, you also need to enter a "2" into P09.91 to transfer the network settings to the comm card.
Also set P09.75 to "0" (Static IP) which is the default in case it was changed to "1" DHCP