ADC_HMI_PE (AutomationDirect) asked a question.
https://www.automationdirect.com/support/software-downloads?itemcode=CLICK
New Features
1) New features for CLICK PLUS CPUs, Pulse Train Output and Pulse Width Modulation.
Improvements
Software
1) Added support for Windows 11.
2) When connected to a PLC the bottom Status Bar in the software will display the connection method: USB, IP Address, COM1, etc.
3) Project Loader, Improved the error reporting when the backup file is not created because the Project File is missing.
4) High Speed Counter Preset Table Outputs are now assigned Nicknames "HighSpeedCount1_Output1".
5) The High-Speed Configuration Windows is reduced in height for use with lower resolution displays, or when Windows Display Scaling is enabled.
6) Navigation Function Tree would display a generic Name for some of the counter modes instead of the assigned Name.
7) Navigation Function Tree would not display if the Preset Table option was enabled for Quadrature modes.
8) All Bits and Registers used by the High-Speed Configurations will now be assigned Nicknames.
9) Address Picker Column and Windows size will now be maintained.
10) Improvement to the module images used in System Monitor and System Configuration.
Firmware
1) Remediation of CISA Vulnerability (ICSA-21-105-02) related to EtherNet/IP.
Fixed Bugs
Software
1) The F1 key did not open the helpfile in several locations: Data Logging, High Speed Configuration, HSC Use Preset, PID Monitor Mode.
2) Windows Alt shortcut for "H" was assigned to menu items Home and Help. These are now changed to "HO" and "HE".
3) Send/Receive did not correctly mark addresses as Used in the Address Picker when using Block Read/Writes.
4) System Monitor might show Analog Input values on the wrong module.
Firmware
1) ASCII Send Instructions with long message length and include Embedded Discrete Messages may send corrupted data.
2) Fixed NTP bug when Scheduled Time Synchronization is set for "Every Hour mm=00". The system time may jump backwards in time 1 Hour and 20 Minutes.
3) Certain DHCP Servers would reject the CLICK Requests and the PLC would fail into APIPA mode on 169.254.x.x
CLICK Software Release 3.30
Thank you for eliminating having to enter our email address before download. That was captcha irritating.
I am prompted to enter email. I do not and do not want to login to the storefront. 😖
Huh. I guess all the prior times I downloaded was while not logged into the storefront. I did not think of that. 🙊
Not sure if there is a more appropriate place to post a suggestion for Click software but I have one:
Trending
You can trend PID tags, but it would be nice to be able to trend any tags. I frequently program first order filters on analog signals and trending the raw and filtered signals is a very valuable tool to adjust the filter constants. That is but one of dozens of uses for trending that would put the Click further along in overtaking the ML1400 capabilities.
Trending like DoMore does is awesome!
See the bottom of this thread -> https://community.automationdirect.com/s/question/0D53u00005YXHWmCAP/pressure-transducer-stabilityaccuracy
Yes, that is handy, but trending as in a big trend chart that is resizable and customizable and can run for long periods (as long as the PC is connected) would be even more handy in some situations.