martinav (Customer) asked a question.
I was hoping for a little better accuracy with stability with this device. Please have a look:
https://youtube.com/shorts/p0h8lQ2RpuM?feature=share
This is a SPTD25-20-1000H transducer, and I was hoping for a pretty solid result to one decimal place. Seems that I would be hard pressed to get a reading stable to the nearest whole number.
There are two of these shown here. They are on the same pipe too. Surprised to see such a different number too. Do they need calibrated?
Maybe I got the wrong idea?? Is hysteresys what I need to look for for a more solid number at an accuracy?
I dont know if I'm even saying this right. Please be gentle.
I think I can manage with this... 100ms looks reasonalbe, and gets me a nice firm xx.x number when rounded.