14svian (Customer) asked a question.

Click output issues

I have a Click C0-02DD1-D output that seems to be not working correctly. The unit is new .

​

I have 24V running through the coils of two 24V relays before running back to the output terminal (Y001) . The Com 2 is connected to the DC negative terminal blocks. I've tested the relay coils and they are functional. I have tested that the Com has continuity to the negative terminal blocks and I have tested that the wire to the Y001 output terminal has continuity to the coils . And I have checked that I am getting 24V to the coils as I should. It seems that when the output is on, the contacts in the PLC are not closing as the should . I forced close a different output (Y003) and tested for continuity to the Com 2 and there was none.

​

Is there something else I might check? Did I get a defective unit? The inputs on the unit appear to be working correctly .

​

Do I need to run 24V to the V+ terminal ???


  • RBPLC (Customer)

    Please post of a picture or schematic of your wiring. It's unlikely that anything is wrong with the unit. It's most likely that the wiring is incorrect.

  • bcarlton (Customer)

    "Do I need to run 24V to the V+ terminal ???"

     

    Yes, just follow the manual diagram.Screenshot 2022-01-08 120617

  • Todd Dice (Customer)

    It's also important to look at the load you're placing on the outputs as they are only good to 0.1 amp at 24-volts. Too high a load can lead to output failure.