Tom@Pton (Customer) asked a question.
Trigger Tag
I would like to start/stop a line trend graph when I have a discreet input indicating a process has started/stopped. The graphs tracks the current, power, or rpm.
I have not been able to get a trigger tag to work.. The bit I have attempted to use changes state at the beginning and end of the process. Minutes to hours apart in duration.
Having it track for 24 hours is a waste.
Assuming EA7/EA9...
Have you looked at the Option tab.
Specifically at [ ] Start & Stop Tag
As much as I have looked, I should have seen it, but some times I can’t see anything that is that obvious.
Thanks, I’ll research it when I get home.
Trigger tag just triggers one reading. I think you're looking for start & stop on the next tab as kewakl mentioned.
The help topic is a bit lacking in this regard.
-for item (t) it states (for the Sample Rate)
but for Trigger Tag, it describes how to fill out the form, without a clear mention that this tag will trigger one sample. (of course, one can infer or learn this, but it is not explicitly spelled out in the topic.)
Hmm, maybe this is a help topic CM244 feature request.
I did come to the conclusion the TT was a one shot deal.
Start Stop Tag should do it. Too obvious
Thank you.