adccommunitymod (AutomationDirect) asked a question.

DL05 modbus to Sureservo

Created Date: January 20,2009

Created By: lrhopper

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I'm working on a cut-to-length application. I'm wanting to use a DL05 RS232 modbus to write parameters in the Sureservo amp for the internal indexer presets(positioning mode). I will be using C-more micro to enter the desired length, RPM, and total pieces to cut. I'm trying to follow the example in the Sureservo manual, but so far most of it is over my head. I already got this up and running using the 8 preset positions and discrete IO to trigger each preset, but I need more than 8 positions. As I understand, I can overwrite a single preset with modbus to be able to cut any length, anytime.


  • adccommunitymod (AutomationDirect)

    Created Date: January 20,2009

    Created by: lrhopper

    I'm working on a cut-to-length application. I'm wanting to use a DL05 RS232 modbus to write parameters in the Sureservo amp for the internal indexer presets(positioning mode). I will be using C-more micro to enter the desired length, RPM, and total pieces to cut.

    I'm trying to follow the example in the Sureservo manual, but so far most of it is over my head.

    I already got this up and running using the 8 preset positions and discrete IO to trigger each preset, but I need more than 8 positions. As I understand, I can overwrite a single preset with modbus to be able to cut any length, anytime.

    Expand Post