adccommunitymod (AutomationDirect) asked a question.

DL06 Analog output wiring

Created Date: October 18,2012

Created By: bmil

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I need to connect an output from a F0-04DAH-1 module in a D0-06DR PLC. I currently am successfully driving two VS pumps from other outputs and the power for those comes from a seperate DC power supply, not the DC available in the PLC. The output will drive a direct coupled valve actuator. My question is how to correctly wire the output to the actuator without harming the PLC. The valve is powered by a 24VAC transformer. The actuator wiring diagram shows one leg of the 24 VAC being connected in common with the PLC output ' - ' signal wire. A dropping resistor is connected between the output ' + ' and ' - ' signal wire. I am enclosing the PDF of the actuator, the wiring I am referencing is on pg 7, fig. 12. Any help/direction is appreciated.


  • adccommunitymod (AutomationDirect)

    Created Date: October 18,2012

    Created by: bmil

    I need to connect an output from a F0-04DAH-1 module in a D0-06DR PLC. I currently am successfully driving two VS pumps from other outputs and the power for those comes from a seperate DC power supply, not the DC available in the PLC. The output will drive a direct coupled valve actuator. My question is how to correctly wire the output to the actuator without harming the PLC. The valve is powered by a 24VAC transformer. The actuator wiring diagram shows one leg of the 24 VAC being connected in common with the PLC output ' - ' signal wire. A dropping resistor is connected between the output ' + ' and ' - ' signal wire. I am enclosing the PDF of the actuator, the wiring I am referencing is on pg 7, fig. 12. Any help/direction is appreciated.

    Expand Post