adccommunitymod (AutomationDirect) asked a question.
Sp1 and sp2 question
Created Date: June 04,2012
Created By: usertodd1
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I was reviewing the High Speed Input/Output modes in the DL06 manual. Instead of using SP2 (which is Always Off) for arguments in the Up/Down Counter code, the example shows NOT SP1 (SP1 is Always ON). Is there a reason to use Not SP1 instead of SP2? Are these equivalent?
Created Date: June 04,2012
Created by: KB1GNI
Someone else should chime in, but I can't see that not SP1 would be any different than SP2. I'd be curious to know if there is a difference and if so, why.
Created Date: June 04,2012
Created by: scott.lawrence
just a guess, but since hitting the space bar automatically adds a NO contact, maybe the SP2 is ADs equivalent to RS5 AFI?
Created Date: June 04,2012
Created by: Do-more PE
There is no difference between a NC SP1 and a NO SP2. It just depends on how you want the logic to look.
Created Date: June 04,2012
Created by: usertodd1
I was reviewing the High Speed Input/Output modes in the DL06 manual. Instead of using SP2 (which is Always Off) for arguments in the Up/Down Counter code, the example shows NOT SP1 (SP1 is Always ON). Is there a reason to use Not SP1 instead of SP2? Are these equivalent?