adccommunitymod (AutomationDirect) asked a question.

xp software

Created Date: March 13,2017

Created By: a agnone

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Don't get rid of the XP software just yet. I keep one or two around for work. Just to share one experience. I found this older H4-Ecom Card I wanted to use. Since i am using it in a local system, it is just fine. Anyhow I did not know the address so i thought I could use my Win7 notebook to find it. Well, that did not go so well. I tried netedit and IPconfig in the new DoMore software and no luck. So knowing XP has IPX available, I went that route and it worked. I changed the address. So I install the Ecom into the system. Plug in the ECOM ethernet port and guess what, I can not read the address. Again i tried both DS6 and DoMore and no luck, nothing, it does not exsist. But since I knew the address I was able to setup the comms and i was able to connect to the PLC and do what I needed to do. If anyone is thinking, yes I had my notebook set to 192.168.000.xxx when I installed the card into the system. I forgot to mention I had to upgrade the firmware while I was attached to the XP computer. Anyone have any ideal why win7 netedit will not pick up on a H4-ECOM, it is not a ECOM100. I did not try the IPconfig that comes with DO More when i finally installed the Ecom card, knowing the address. I did not have the time to do it. I will try it tomorrow or when I get back to work. Tomorrow is a big storm coming so I do not think I will go in tomorrow


  • adccommunitymod (AutomationDirect)

    Created Date: March 13,2017

    Created by: a agnone

    Don't get rid of the XP software just yet. I keep one or two around for work. Just to share one experience. I found this older H4-Ecom Card I wanted to use. Since i am using it in a local system, it is just fine. Anyhow I did not know the address so i thought I could use my Win7 notebook to find it. Well, that did not go so well. I tried netedit and IPconfig in the new DoMore software and no luck. So knowing XP has IPX available, I went that route and it worked. I changed the address. So I install the Ecom into the system. Plug in the ECOM ethernet port and guess what, I can not read the address. Again i tried both DS6 and DoMore and no luck, nothing, it does not exsist. But since I knew the address I was able to setup the comms and i was able to connect to the PLC and do what I needed to do. If anyone is thinking, yes I had my notebook set to 192.168.000.xxx when I installed the card into the system. I forgot to mention I had to upgrade the firmware while I was attached to the XP computer.

    Anyone have any ideal why win7 netedit will not pick up on a H4-ECOM, it is not a ECOM100. I did not try the IPconfig that comes with DO More when i finally installed the Ecom card, knowing the address. I did not have the time to do it. I will try it tomorrow or when I get back to work. Tomorrow is a big storm coming so I do not think I will go in tomorrow

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: March 13,2017

    Created by: BobO

    One possibility is the default order of Ethernet adapters. Older versions of Windows sent broadcasts out every port. Newer versions do not. From NetEdit, be sure to select the correct adapter from the menu. In many cases that is required to work properly.

  • adccommunitymod (AutomationDirect)

    Created Date: March 13,2017

    Created by: a agnone

    I will check that next time with NetEdit. I do remember IPconfig in Do More asking which adapter. Not sure why IP config did not work either. I tried putting my notebook adapter to Obtain IP address automatically. Also tried several manual settings. which way is preferred or does it matter?

  • adccommunitymod (AutomationDirect)

    Created Date: March 14,2017

    Created by: BobO

    I will check that next time with NetEdit. I do remember IPconfig in Do More asking which adapter. Not sure why IP config did not work either. I tried putting my notebook adapter to Obtain IP address automatically. Also tried several manual settings. which way is preferred or does it matter?

    Doesn't matter as long as the IP addresses are on the same logical network (Netmask & PC Address == Netmask & ECOM Address). The key is making sure that the config broadcasts are going out the port where the ECOM is connected. In NetEdit, on new Windows, in many cases it won't work until you select the right adapter.

    Expand Post