adccommunitymod (AutomationDirect) asked a question.

Automation Direct GS-ERDV

Created Date: September 02,2016

Created By: binary01

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I am slowly teaching myself Automation Direct, recently I purchased 1 GS-EDRV 100 and 1 GS-EDRV from ebay. I configured the GS-EDRV 100 easily but I a cannot find the IP address of the GS-EDRV using NetEdit3,played around with the dip switches, even used Advanced IP scanner and nothing. When powered up the RTS and TDX led blinks, RXD led on steady, link led on steady and the Active led blinks ever so often. Is there something i didnt do? Any assistance is much appreciated


  • adccommunitymod (AutomationDirect)

    Created Date: September 02,2016

    Created by: binary01

    I am slowly teaching myself Automation Direct, recently I purchased 1 GS-EDRV 100 and 1 GS-EDRV from ebay.

    I configured the GS-EDRV 100 easily but I a cannot find the IP address of the GS-EDRV using NetEdit3,played around with the dip switches, even used Advanced IP scanner and nothing.

    When powered up the RTS and TDX led blinks, RXD led on steady, link led on steady and the Active led blinks ever so often.

    Is there something i didnt do?

    Any assistance is much appreciated

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: September 02,2016

    Created by: plcnut

    Are all the dip switches off?

    How did you configure the the GS-EDRV if you do not know it's IP address?

    Is there a router on the network?

  • adccommunitymod (AutomationDirect)

    Created Date: September 02,2016

    Created by: binary01

    Thanks for the response Plcnut.

    I have One GS-EDRV 100 which i configured with no problem at all

    and 2 GS-EDRV( the older one 10base) which i cannot see the ip address

    All dipswitches are off

    No router on the network.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: September 02,2016

    Created by: plcnut

    I should have read your first post more carefully :enbarrased/frown:

    Are you using a crossover cable straight to your PC?

    Also, did you cycle power on the unit?

  • adccommunitymod (AutomationDirect)

    Created Date: September 02,2016

    Created by: Mike Nash

    You can also check the FAQs here: http://www.hosteng.com/FAQFiles/EDRV.htm

    I have no EDRV experience, but NetEdit has been "quirky " at times requiring me to select the network card, or choose IPX instead of TCP or vice versa.

  • adccommunitymod (AutomationDirect)

    Created Date: September 02,2016

    Created by: binary01

    Plcnut there is nothing to be embarassed,about believe me.

    Windows & does not have IPX

    cycled the power and even have a stride ethernet switch, all my ethernet cards are read from netedit except the GS EDRV,

    I am thinking if something is wrong with the converter but the error light is OFF.

  • adccommunitymod (AutomationDirect)

    Created Date: September 06,2016

    Created by: GKiser

    binary01, When you use NetEdit, choose from the menu, Network --> Adapter and pick something besides Default. Does that cause the GS-EDRV to show up?

  • adccommunitymod (AutomationDirect)

    Created Date: September 07,2016

    Created by: binary01

    Thanks for the response Greg.

    I found the problem, It had an different IP (and maybe subnet).

    I used my windows XP pc and enabled IPX and found the IP(10.20.253.14)but could not see the subnet, reset to factory default and then assigned my new IP.

    Thanks everyone.