adccommunitymod (AutomationDirect) asked a question.

Bad c-more ea7-t10c

Created Date: September 30,2016

Created By: carmusic

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Hi i have a ea7 interface that started to loose its operating system (no changes have been made) . Every time it is disconnected and powered it shows black screen with warning No system found, please put in program mode... I have to use the reset tool, it then shows safe mode menu. After i must clear memory via cmore software and i can download the program. (if i dont clear memory, it says unknow panel, 0.0.0.0 firmware, i can install new firmware but it crashes when rebooting showing the black screen) Battery shows 3.1 volt so i assumed it is ok. Everything works normally until we lost power for few seconds. Panel is from 2014. is there other thing to check? firmware is version 2.78


  • adccommunitymod (AutomationDirect)

    Created Date: September 30,2016

    Created by: carmusic

    Hi i have a ea7 interface that started to loose its operating system (no changes have been made) . Every time it is disconnected and powered it shows black screen with warning No system found, please put in program mode... I have to use the reset tool, it then shows safe mode menu. After i must clear memory via cmore software and i can download the program.

    (if i dont clear memory, it says unknow panel, 0.0.0.0 firmware, i can install new firmware but it crashes when rebooting showing the black screen) Battery shows 3.1 volt so i assumed it is ok. Everything works normally until we lost power for few seconds. Panel is from 2014. is there other thing to check? firmware is version 2.78

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: September 30,2016

    Created by: kewakl

    FW/SW 2.78 SP1 is available.

    2.78SP1 DOES NOT FORCE A FIRMWARE UPGRADE AS ANY REV DOES.

    Do you have any cards/memory modules installed?

    Is the DC 24V clean, well grounded?