adccommunitymod (AutomationDirect) asked a question.

C-More Very Small Real Numbers

Created Date: May 15,2009

Created By: Dan @ CHP

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

When displaying small magnitude real numbers using the Numeric Display object, the panel will display the value in scientific notation (23 E-3, etc.) rather than rounding to -1, 0 or +1 as appropriate. The minimum value that is properly rounded is related to the number of decimal places selected in the numeric display object. Is there a way to achieve the desired results? I 've developed some clumsy code in the PLC to superimpose a text "0 " over the numeric display object but it seems there should be a better way.


  • adccommunitymod (AutomationDirect)

    Created Date: May 15,2009

    Created by: Do-more PE

    You can disable Exponent Notation in the Panel Manager. You can find it in the General section in the same place that you set the Panel Type.

  • adccommunitymod (AutomationDirect)

    Created Date: May 18,2009

    Created by: Dan @ CHP

    Works great. Thanks.

  • adccommunitymod (AutomationDirect)

    Created Date: May 15,2009

    Created by: Dan @ CHP

    When displaying small magnitude real numbers using the Numeric Display object, the panel will display the value in scientific notation (23 E-3, etc.) rather than rounding to -1, 0 or +1 as appropriate. The minimum value that is properly rounded is related to the number of decimal places selected in the numeric display object.

    Is there a way to achieve the desired results? I 've developed some clumsy code in the PLC to superimpose a text "0 " over the numeric display object but it seems there should be a better way.

    Expand Post