kewakl (Customer) asked a question.
Solo StopRun / switch
Please describe the interaction between the Stop/Run switch and the Stop/Run register.
(1) Run/Stop switch in Run, issue Stop via comms, the Run/Stop switch does not override the previously written Stop mode register value (module does not enter Run mode)
(2) Run/Stop switch in Stop, issue Stop via comms, the Run/Stop switch does override the previously written Stop mode register value (module returns to Run mode)
Also, maybe blink the RUN lamp when scenario (1) is true