kewakl (Customer) asked a question.

Solo StopRun / switch

Please describe the interaction between the Stop/Run switch and the Stop/Run register.

 

(1) Run/Stop switch in Run, issue Stop via comms, the Run/Stop switch does not override the previously written Stop mode register value (module does not enter Run mode)

 

(2) Run/Stop switch in Stop, issue Stop via comms, the Run/Stop switch does override the previously written Stop mode register value (module returns to Run mode)

 

 

Also, maybe blink the RUN lamp when scenario (1) is true