jvfred (Customer) asked a question.
Is there any chance a full version of Codesys will be released for the P2CDS-622? I miss the Alarm Manager and Symbol Configuration in the full version that the P2 lacks.

jvfred (Customer) asked a question.
Copyright © 1999-2023 AutomationDirect. ALL RIGHTS RESERVED
Apologies for the late response. The P2CDS-622 is running the full version of Codesys. Unfortunately it does not support the Alarm Configuration and Symbol Configuration like I mentioned in the previous post.
If this changes in the future I'll post an update.
Our next Codesys product will have support for these features and much more compared to the 622 in the near future.