Nixter (Customer) asked a question.

StrideLinx Cloud Line Graph: what syntax and length limit does the formula field allow?

In StrideLinx Cloud Studio, the Line Graph component has a formula field for each historical line. I'm not asking about the data tag's Formula setting in Fleet Manager (mean, max, last, etc.). I mean the per-line formula field in the component settings, which overrides the variable's factor for that graph only.

 

As far as I can tell, this comes from IXON Cloud 2.65.3 (June 2026). That release added formulas, instead of just factors, to historical metrics components, with Celsius to Fahrenheit given as an example.

 

My questions:

Operators: Which operators are supported? Is it just + - * / and parentheses, or also ^, %, bit-wise logical operators (AND, OR, XOR with masks) or anything else? Currently their documentation on their website (https://support.ixon.cloud/s/article/Studio-components---Historical-Metrics-components) shows only very rudimentary addition, subtraction and parentheses are support. I'm hoping that there is actually more, or more planned for the future.

 

Functions: Are any functions available, such as abs, min/max, round, sqrt or log?

 

Length limit: What is the maximum formula length in characters?

 

Documentation: Is there a support article that covers this?

 

Thanks,

Nick


  • ADC_PLC_ENG (AutomationDirect)

    This has not been implemented in the StrideLinx sector. If and when it is we will add to our documnetation.

     

    Thanks!

    Selected as Best
  • ADC_PLC_ENG (AutomationDirect)

    This has not been implemented in the StrideLinx sector. If and when it is we will add to our documnetation.

     

    Thanks!

    Selected as Best
  • Nixter (Customer)

    Thanks for the answer. After checking the IXON website, I surmised that only rudimentary +,-,*,/ were available for forumlas.

    Hopefully, in the future they will add bitwise logical operators. Those would be #1 on my wish list.