ElecSparky (Customer) asked a question.
I have a request or suggestion that would be a benefit to remote connections where if you had the PLC program file in the micro SD slot on a card, the operator or someone in the plant could access the built in web server to download the project file right from the card if the memory was lost? Say if the party that built the controller were not available.. ie:weekend/holidays. This is nice on the Cmore to have that backup, would be great on controller also.
Thanks for the suggestion! I will forward your suggestion to the Productivity Management team.
As another option the operator could use PSLoader to load a .adprx file that is generated from the software and load this to the CPU via an Ethernet or USB connection.
https://www.automationdirect.com/support/software-downloads?itemcode=PS%20Loader