georgeksu (Customer) asked a question.

I downloaded the click PLC software v3.92 on my Raspberry Pi 5 which is a Linux based operating system. But the click software won't work, it says "visual C++ 2015 install failed". Has anyone had this problem too? Any solutions?

  • ssweber (Customer)

    Are you trying to install via Wine? Click is a windows application.

  • georgeksu (Customer)

    Yes, I installed via Wine. Pi operating system says it has all the window's components. I just want to use Pi as a programming device.

  • K Price (Customer)

    Yes, a Windows application, in particular, the Supporting Operating Systems listed for Click v3.92 is: Windows 10, and Windows 11. I worked with someone who "runs a Windows Virtual Machine" on a Linux-based computer (though not for Click). Do you know if your computer is capable of this? Sorry, I do not know, I have never "run a Windows Virtual Machine on Linux". Perhaps ADC tech support, or other customers, can verify if it is possible to run Click software on a "Windows Virtual Machine".

    Expand Post
    • z28z34man (Customer)

      Is this on an x64 processor? The raspberry pi is running on an ARM CPU with a reduced instruction set. I could see the software not being compatible with an ARM CPU even if it works in Linux with WINE

      • PouchesInc (Customer)

        Oh that's true, good catch. I forgot about the CPU aspect of it.