RedBarn (Customer) asked a question.
For some reason when I am trying to upgrade from Pro Suite 4.6.2.2 to the newer Pro Suite 4.7.2.4 (or 4.7.1.5 or 4.7.0.47), a couple of my timers start bouncing their values. These are standard TMR timers. Using hour units. And the value bounces up and down several 100 "hours" every second. No idea what to try in order to fix this. Delete the rung and make a new one? Can I trust that the other couple dozen or so timers in my ladder are not also randomly corrupted? Adding an always off contact at the enable seems to stablilize it. The enable signal does not trigger a counter.
Older P2-550 on a P2-07B. Was on older firmware but have upgraded to 1.3.0.6 and 1.0.16.0.
Or development team discovered a bug that was introduced in Productivity Suite v4.7 that is affecting the Reset pin of the timer instruction and causing the issue that you are seeing. The bug fix will be in the next release of the software. In the meantime, the only work arounds are to either fall back to Productivity Suite v4.6 or disable the Reset pin of every timer and add code to reset the current timer value to the reset value.
We sincerely apologize for the inconvenience this has caused you.