FAHoutdoors (Customer) asked a question.
Analog Bar Thickness Feature Request.
Could there be a better way to allow the thickness of the analog bar to be changed, maybe in the options for the object property? Right now you can only do it by increasing the height of the analog bar object which almost makes me think it's a bug or unintended behavior, but I really like being able to make that bar thicker, as the default is pretty thin. Picture below to demonstrate what I mean.
There is no current way to just change the thickness. I see what you are saying.
The Analog Meter and Bar Meter both get thicker with the size. That is not very flexible. Having a setting similar to what the Slider object has is a good idea.
Oh yeah I forgot the slider had a "track size" option on it even though I used that just yesterday. That would be a good way to handle it. Thanks for taking it into consideration.