Cap (Customer) asked a question.
How to Lock a Line to Horz or Vert in V9?
Forcing myself to use the V9 Software.. However I'm not seeing a way to Lock a Line to Horz or Vert ( Like Previous Ver Did ) so when I'm making Charts or Tables using the Line, they wander.. I can Snap to Grid. but I'm not always using that feature..
Just Checked. Its only V9.0.. Has this been Fixed in Later Ver.. I hate Swapping Versions, Cauze I have to do it to all my Screens when I do.. Else I get myself in a Bind Sometimes in Production..
Thanks..
Cap
The setting is removed and it is accomplished though the keyboard and mouse.
See Help File "Shape Size and Rotation" Topic CM373 for more details.
Mouse + SHIFT: change angle in 15° increments.
@Cap (Customer) Also, based on your application, give the Grid object a try. Look at the help file. It has a lot of capability for arranging objects.
Took a while to find it.. This is what I found..
file:///C:/Program%20Files%20(x86)/AutomationDirect/C-more%20HMI%20Ver9.00/Help/Content/373.htm?Highlight=CM373
Granted it was already in MY Computer.. However finding and NOW Understanding it all will take a While..
Love Progress.. Hate Change..
Thanks..
Cap