Cap (Customer) asked a question.
V9.0 and I want the Old Graphic Library
I'm Struggling through V9 C-More.. I'm Getting it, however I'm liking the Availability of more Graphics on the Older Versions.. and my Projects are Imported, so I'm wanting 'Graphic Similarity'.
How can I Change the Library Options to the Older Version from in V9?
Thanks..
Cap
@Cap (Customer) are you talking about the graphics in the new Graphic Studio? If you can be more specific with some screen shots of what yo are looking for, we may be able to get those put in.
We cannot use the specific graphics from Symbol Factory because of licensing.
If you are talking about the graphics in the Graphic Library, those have not changed. Again, a screenshot of what you are referring to would help us understand. Thanks
We cannot use the specific graphics from Symbol Factory because of licensing.
How do we continue without the Symbol Factory Easter Eggs?
You could clip the symbols from the old Symbol Factory.
https://softwaretoolbox.com/symbol-factory offers licensing. I do not know if this could help you.
I was referring to Symbol Factory.. I was wondering if I could link my copy of V9 back to a Copy of v6 where I have Symbol Factory..
I can I purchase a License for Symbol Factory and somehow inport it into V9?
Else it Looks Like it'll have to be Screen Grabs, and Cut and Paste?..
Thanks..
Cap
There is no way to use Symbol Factory in V9.
You can create objects in V6. Save to the object library. Copy the library files from here:
C:\Users\rthornton\OneDrive - Automationdirect.com Inc\Documents 1\AutomationDirect\C-more\Library\User Object
To here:
C:\Users\rthornton\OneDrive - Automationdirect.com Inc\Documents 1\AutomationDirect\C-moreCM5\Library\Object Library\User Items
And use that object from the Object Library in the V9 project.
I've been Opening the Object I want in Symbol Factory.. Then Copy Right Click Copy.. Past into Paint.. Then Manipulate in Paint to get the Coloring and the View ( Left Right Upside Down ) then Save as BMP into a File, then Fetch from V9 My PC Button..
I had to make some Pneumatic Actuated Rotary Butterfly valves for my Other C-More Screens.. So that is the Technique I used then..
It'd be TOO simple if I could Import Symbol Table.. But I understand the License thing..
Thanks..
Cap
If you are going to be editing bitmaps, png, jpg, etc. I highly recommend Paint(dot)net:
www.getpaint.net
It's like photoshop for amateurs. It is very easy to use and has tons of keyboard shortcuts plus the power of layers, distortions and there are pllug-ins like perspective that I frequently use to take a picture of a panel, a data plate I can barely see, or a drawing and "make it lay flat".
https://forums.paint.net/forum/7-plugins-publishing-only/
I contacted Symbol Factory to have them look for Options with V9.. This is the Reply..
Cap hi,
Thank you for clarifying. That makes sense.
Since C-More V9 no longer includes Symbol Factory as a native graphics library option, the best next step is to test Symbol Factory directly and confirm whether exporting standard image formats, such as PNG or JPEG, works cleanly for your C-More V9 workflow.
You can download the Symbol Factory demo here:https://downloads.softwaretoolbox.com/demodnld/237/Symbol_Factory_Universal.exe.
We are fairly confident this should work, since Symbol Factory allows graphics to be exported as standard image files that can then be imported into other applications. Once you test it, please let us know if it gives you the workflow you need.
Here is the link for the Symbol Factory page if you are interested in purchasing: https://shop.softwaretoolbox.com/Symbol-Factory-Universal-Single-User-License-incl-1-Year-Support-Maintenance-Agreement. If the demo works well for your C-More V9 use case, let us know and we can process the order right away.
Thanks!
Sarah
I have not tried this yet, because I want my Demo Version to be active longer then just this one Project.. The Software and License is ~$700.. More than I want to pay Out of Pocket Un-rembursed presently.
My present project is just making my old Graphics ( With a little Touch Up ) run under V9, as the Screen was Changed in Size due to System Complexity..
I'm looking foreward to the Strip Chart Options in V9.. However that will require my Screens to be changed to CM5's.. Presently EA-9's.. Except for TWO screens added this last Year..
Cap
The easiest approach is:
Open any older C-more version (8.x or 6.x)
Add a bitmap button (or static bitmap)
Select "Symbol" to launch Symbol Factory. This is a fully licensed version. We intend to maintain the license as part of long-term support for V8.
Select your image - click OK
Symbol factory adds the image to your Windows Clipboard
Then in V9, most objects allow you to add images, just click the "Clipboard" option.
This will "Paste" the clipboard image into your V9 project
Our goal is to continue to enhance the Graphics Studio image library in V9. We also intend to add an SVG import option in the near future so you can add your own custom graphics to Graphic Studio.