Cmore 5 T7W terminal - Version 9.0 Pushbutton / Indicator is extremely slow to respond to push button pressing
Cmore 5 T7W terminal - Version 9.0 Pushbutton / Indicator is extremely slow to respond to push button pressing and the state change indication of the button on the display. Talking like 6 to 10 seconds to change, button to PLC signal is nearly instant. Compared to version 8.26 which was nearly instant the button was pressed the indication changed. Also buttons with indication tags from the PLC are very slow to indicate the PLC tag change. Using Serial link at 38K rate for comms and do not have Ethernet available as it is utilized for another purpose.

Which PLC are you communicating with?
Knew there was a detail that I forgot...AB Micro870 via onboard Serial port. Same setup using 8.2X and have not experienced this tremendous delay. recreated buttons from scratch within V9.0 and still no difference, same long delay in display, button is nearly instantly seen in the PLC data table.