Tom@Pton (Customer) asked a question.
Latest C-MORE v9
Lots of good stuff and I'm just getting started.
Simulation mode doesn't appear to allow me to turn ON inputs.
Is it in there somewhere?

Tom@Pton (Customer) asked a question.
Lots of good stuff and I'm just getting started.
Simulation mode doesn't appear to allow me to turn ON inputs.
Is it in there somewhere?
Copyright © 1999-2023 AutomationDirect. ALL RIGHTS RESERVED
@Tom@Pton (Customer) I hope you meant "Ver.9.0" in the title and not EA9; 😁
Only two things changed in the Simulator:
Everything else is till the same.
Are you not seeing the control panel? Or does clicking on the ON/OFF not do anything?
clicking on the on/off doesn't do anything
Referencing a CLICK the X discrete inputs cannot be cycled. C discrete can.
Referencing an AB ML400 one for the signed integers did not transfer, but I need to look at that closer. Decimal value for O:0.0
The same HMI project is used to reference two CLICKS and the AB.
...ML1400...
The issue with triggering CLICK inputs from the simulator has been fixed in V9.02 and is available on the downloads site:
Software & Firmware Downloads
https://www.automationdirect.com/support/software-downloads?itemcode=C-more%20CM5%20Series#
Got it.
Thank you!
let us know....😊
Yes, they fixed it!!😊
Thank you for your follow up!