Cap (Customer) asked a question.
I went through a few Gyrations to get the MAC Address from my Last Batch of Clicks.. This time I'd like to not have to set up a Router for the Clicks, just to get the MAC Address from the Connection..
Is it SOMEWHERE accessible from the Software that is Connected to it?.. V3.80
Cap
Without some research, I do not know when this capability was added, but in Version 3.92
There are (2) ways to see the MAC from the connected Click.
1) PLC > Online Project Information... > Connect (shown in hex, for example: 00:D0:7C:12:97:8A)
2) In Data View, SD188 thru SD193 (shown in dec, for example:
SD188: 0
SD189: 208
SD190: 124
SD191: 18
SD192: 151
AD193: 138