I have a Code CR950 on a CM5 display via USB, and I have the condition where rapid scans will trigger a 'shift' on scans where numbers send the shifted characters. Once triggerd, all number come through as the shifted counterpart. The only way I have found to clear this is a full power cycle. I tried to scan the reset QR Code (M20112_02) to reset the reader, and that didnt fix the issue. So, i'm not sure where the issue lies.
I did find a delay for repeat scanning that helps prevent the issue (M20219_02). It will refuse to re-scan the same code, but if different codes are scanned too quickly, the problem repeats. So, I actually dont know if the problem is in the reader, or the CM5.
Thanks!