FAHoutdoors (Customer) asked a question.
I transferred a project from the latest 8.X release to Beta 3 just to mess around with it. On one screen I have some static text with a red background that covers some analog gauges that says "No Signal" iff the mA signal drops below 4 mA. this worked fine on the V8.X release but didn't seem to work at all on the beta version. but literally as I was writing this post I turned off and back on the visibility option on all the objects and rewrote it and now it works perfectly? Now I'm wondering if I should even post this at all haha.
I will say it really does appear to be at least noticeably snappier then 8.X even with a tiny program, and I know 8.X along with the CM5 was already so much snappier then the EA9 and 6.X software so I'm pretty happy so far with it from that perspective.