Elliot (Customer) asked a question.April 20, 2026 at 1:51 PMcm5 hmi. Project uses usb4 and screen doesnt have that option. How to fix?Expand PostC-More
ADC_HMI_PE (AutomationDirect)2 months agoThe USB4 is only available on the CM5-RHMI, headless unit. If you are using a different model, you will need to change the model number in the Panel Manager.Expand Post
The USB4 is only available on the CM5-RHMI, headless unit. If you are using a different model, you will need to change the model number in the Panel Manager.