Scott1234 (Customer) asked a question.

Error in Grouping

Hi

I found out when grouping a row of buttons or grouping a row of numeric displays when you try and slide to move to a specific spot after grouping or try and edit a single button or numeric display the software closes...if you didnt save you lost your changes you made..


  • ADC_HMI_PE (AutomationDirect)

    @Scott1234 (Customer)​ Which version are you using?

     

    Did you start a new project or are you using a project from a previous Beta? It is best to start from scratch or convert from V6.80 or V8.26. Things may change from Beta to Beta.

     

    I am unable to duplicate this in the latest internal release.

  • Scott1234 (Customer)

    I converted a project that i had started and wanna some upgrades but as i continue to build on it i found this problem.. Is the duplicating something we wouldnt be able to do? or is that a software issue?

  • ADC_HmiClicK_PE01 (AutomationDirect)

    Thank you, what version of software did you start the project in. Sorry about all the questions, but the closer we can get to recreating your exact steps, the easier it is to reproduce the problem.

  • Scott1234 (Customer)

    Hi Sorry i didnt see this response..

    i Started this project in 8.24V but the grouping i never had an issue with except when i started using the new beta 9.0

  • Scott1234 (Customer)

    Could i send you the Project via Email than you could have a look and see if you can group the Gal/day column without freezing the software..Youll see what i mean once you see the project..