tom.fisher2000 (Customer) asked a question.April 2, 2026 at 3:29 PMcan iuse a cm5 with a slm1Expand PostProcess ControlC-More
K Price (Customer)3 months agocheck out this tech note:https://www.automationdirect.com/support/question-answer?techId=6057 Expand Post
ADC_Tech_03 (AutomationDirect)3 months agoYes, the CM5 can communicate over Modbus RTU to the SLM unit. There is a built in driver for the Solo units to make tag setup easier as well. See these help file links (initial setup) and (addressing). Expand Post
check out this tech note:
https://www.automationdirect.com/support/question-answer?techId=6057
Yes, the CM5 can communicate over Modbus RTU to the SLM unit. There is a built in driver for the Solo units to make tag setup easier as well. See these help file links (initial setup) and (addressing).