MechE87 (Customer) asked a question.

Replacing P1AM-200 Bootloader with RS485 compatible one

I am interested in replacing the stock bootloader with one that is compatible with the RS-485 serial shield. Do you have a work flow or instructions on how to reprogram the bootloader section? I need to be able to perform in field updates, and my only connection to the device will be over RS485.


  • FACTS_AdamC (AutomationDirect)

    Hey @MechE87 (Customer)​ ,

     

    We do not provide an RS485 compatible bootloader. While it could be possible to create this yourself, it will take a decent understanding of microcontrollers and their flash and carries the risk of bricking your device if implemented incorrectly.

     

    Thanks

    Adam

    Expand Post
  • MechE87 (Customer)

    Thanks for the clarification. With the risk of bricking the device, is there an access port to SWD interface in case that happens? This would be going into a place that doesn't have access to USB if updates are needed and I'd prefer not to have to replace the main controller if an update or feature is needed.