WadeD (Customer) asked a question.

Disable option for objects

I would be nice if there was a disable option for the object like pushbuttons, call recipes, numeric entries and the sort. This way the object is still visible but faded and not active. Instead I have to use visibility option (which I don't particular like) or layer it with other objects and using the visibility option. Such a pain sometimes. A disable feature would effectively stop all this, I believe. No more hiding or layering or creating events. Another cool feature would be to have nested visibility options. Kinda like the event manager where you could but AND or OR tags as part of the visibility option, but would really like to see a disable feature.


kewakl likes this.