Can I add a remote display as a tachometer for display purposes only to my GS2-45P0? Need to see line speed 200' away from main drive and drive supplied display. No programming needed, just visual representation of what the main remote is seeing

Again this is only to display line speed in rpm. 110vac is available to power display. Cat 5 cable or hard wire is acceptable. Easier the better. I am definitely not a seasoned electrician on this level


  • K Price (Customer)

    One way, fairly straight-forward, would be to use the analog output (0-10VDC) from the GS2 and run a cable to a panel meter at your remote location (assuming the analog output is not being used).