ADC_HMI_PE (AutomationDirect) asked a question.
C-more CM5 V9.0 Beta3
Thank you for your feedback on Beta1 and 2. We have fixed the reported bugs and others reported internally.
We are happy to open up Beta testing for CM5 Version 9.0 Beta 3. We hope you enjoy the changes and improvements we have made to the software and features.
The software can be downloaded here:
https://www.automationdirect.com/support/software-downloads?itemcode=C-more%20CM5%20Series
Let us know what you think. Please do not contact Tech Support. Report any issues here on this Community page. Create a New Thread please.
--This Beta is available for trial, testing, and training purposes only--
--Not for production use--
Fixed Bugs
1) Inc/Dec object – background color does not have a No Fill selection
2) Embedded Tag - Numeric - Justify defaults to Leading Zeros. This should default to Leading spaces
3) Slider – Some colors not converting correctly
4) Adjust Display - Button Back Color not converted correctly
5) SYS Copy LogTo%device% - no error if device is not present
6) Bar Meter not converting well
7) Line trend - When there are many pens, the legend cuts off the names
8) Recipe Sheet - Recipe Sheet changes are not saved when leaving edited Recipe Sheet
This release contains hundreds of improvements; we've added a few new objects and consolidated many of the similar objects.
- This release is FAST! The runtime is up to 250% faster to render complex screens.
- We have also added some major new capabilities:
- A New Log Manager which allows you to configure a log process independently from a trend line
- We've rewritten the Trend Line and added Dual Y-Axes, new controls, pinch to zoom and swipe to scroll
- Added Tag based range control to the sliders, analog meters, bar graphs and line charts
- A new Find/Replace to help swap tags, and labels on selected groups of objects
- Support for MELSEC FX5 PLCs and Omron NJ/NX Ethernet/IP
- We've built a new Graphics Studio with all SVG based images which scale and enable tons of new capabilities.
- An object search -no more scrolling through pages of controls to find that one special tool
- A new color picker with eye dropper to select any color available in Windows
- Many improvements to the project Simulator
- Supports conversion from V6.80 or V8.26 (Probably more, but that's why we're testing)
--Limitations/Known Issues--
- We are still rewriting the help files - None of the help buttons work
- EA9 imports with large numbers of tags - some tags may not be imported
- V8.26 to V9.0Beta2 Fonts may not convert correctly.