psteele (Customer) asked a question.
Any AD products that offer 1:1 NAT?
I really want to stop using AB's 1783-NATR devices. Way too expensive for what they do. I've done the Mikrotik and Ubiquity router thing, which is great from a cost standpoint, but more complicated than I would like. I've also looked at MOXA's NAT-102 devices, and the Skorpion routers from Contemporary Controls as well as a few others but would love to have a Stride product that could do 1:1 address translation in a straightforward manner. Has anyone tried this with any of the Stride products? Is it even possible?
No. ADC doesn't currently offer anything that would work for this but your post has been sent to the product team for consideration.
Thanks for posting.
Thanks for the answer.
If it helps to sell this to your team, in the facility that I am currently at, we have over a dozen devices installed doing 1:1 NAT at the moment. Just about every OEM system we get (packaging equipment, robotic systems, refrigeration controls...), gets one of these so we can interface their systems into our plant-wide control network without having to mess with the OEMs internal network or devices.
+1 for a SIMPLE 1:1 Nat
Cap
I will add another +1. I currently use Ubiquiti EdgeRouters and they work well enough but it would be nice to have something din rail mounted and powered from 24V