Jason Waldner (Customer) asked a question.
Can the CMore CM5-RHMI get controlled by a web-app.
When I sign into my IP on a web browser a few options show up, one of which is a web-app or something like that but when I try to follow thw instructions I can't get it to work. Would anybody know how to create a web-app.
Are you trying to connect remotely? In the C-more software, go to Setup/Panel Network
Enable the Web Server function, then also enable the Remote Access. There are a few security options at the bottom of the screen. Download the project
Then go to the IP address of your panel, and select Remote Access
At the op, there is a link "a. Built-in Ethernet Port1 (IP:192.168...)"
If you click that, it will download an applet that will let you control the HMI from your PC.
You can also download the Remote HMI app on the Apple or Google store to control your HMI
I'm trying to connect it to an Apple Mac
I don't have a Mac here to test, but can you try running the Remote HMI app from the Apple app store? If your Mac is using an Apple Silicon M1-M3 chip it may work.