EthernetJP (Customer) asked a question.

Productivity Suite 4.5.0.34 Freezes When Interacting With Data View

Installed this version today to take advantage of the new User Defined Instruction feature. When I attempt to expand a UDT member or array in the Data View, the entire Productivity Suite freezes and must be closed by ending the task in Task Manager. This has happened 3 times so far, always immediately after trying to expand a Data View entry.


  • ADC Community_02 (Automationdirect.com)

    So far we have not been able to reproduce the issue you are seeing. Can you PM a copy of your project so we can try and duplicate? Thanks!

    • EthernetJP (Customer)

      Thanks for the response! Just sent the project.

  • kewakl (Customer)

    I have not experienced this. Can you some PC specs, CPU/speed, GPU, RAM size.

    Not to hijack this thread, the weird GUI interactions that I have experienced :

    when typing an instruction mnemonic into a rung, the software fails to recognize the mnemonic's second character.

    It is like the GUI is spending a lot of time determining what (*) I mean to type while ignoring WHAT I TYPE!

     

    (*) to populate the matching instruction dropdown list

    Expand Post
    • EthernetJP (Customer)

      I have experienced a very similar issue in versions before 4.5 as well. Earlier this year, I had some highly repetitive code that looked at several hundred modbus registers and alarmed if they were outside a certain range. I decided to write a python script using pyautogui to enter the ladder instructions. What I kept running into was that the first character I typed would occasionally be "seen" by the IDE as having been pressed twice, so I ended up doing something like this for every instruction:

      *type first character of mnemonic

      *backspace

      *backspace again!

      *type the entire mnemonic

      Expand Post
    • EthernetJP (Customer)

      PC specs:

      Dell Precision 7780

      Processor: 13th Gen Intel(R) Core(TM) i7-13850HX (2.10 GHz)

      RAM: 32.0 GB

      GPU: NVIDIA RTX 3500 Ada Generation Laptop GPU

       

  • ADC Community_02 (Automationdirect.com)

    @EthernetJP (Customer)​ We are unable to reproduce the issue with your provided project. Please PM me the two below items.

     

    1.) Create a system report. Help -> Create a system report. This has additional files and logs that could provide help to our developers.

    2.) Provide a short video of the issue.

    • EthernetJP (Customer)

      Yesterday I was able to reproduce this issue very consistently. Ended up being 4 times in total.

       

      Today, I can't make it happen.

       

      The day before I installed Productivity Suite 4.5.0.34, I installed Java SE Development Kit 25.0.1.

      I uninstalled that this morning and am now unable to reproduce this issue.

       

      Maybe just a coincidence...

       

      If it rears its head again and is reproducible, I'll screen record and send that along with a system report.

      Expand Post
      • ADC Community_02 (Automationdirect.com)

        Appreciate the update — glad to hear the software’s working now!