M.Farahani (Customer) asked a question.

CP342-2 / CP343-2 (ASI Configuration)

 

Hello everyone,

I’m currently working with SIMATIC Manager 5.5, Service Pack 2, and I’m trying to map an AS-Interface (ASI) network for two Siemens modules:

  • 6GK7 342-2AH01-0XA0 (CP342-2)
  • 6GK7 343-2AH01-0XA0 (CP343-2)

The issue is that in my hardware configuration, I only have access to two tabs: General and Addresses. The crucial ASI-related tabs (required for proper network mapping) are missing.

I’ve searched online for the corresponding GSD files (siem8093.gsd, siem80d6.gsd, siem8095.gsd, siem80d7.gsd), but all official and unofficial sources are either offline or return 404 errors. I don’t have an active Siemens support contract, so Siemens cannot provide the files directly.

If anyone here has these GSD files for CP342-2 / CP343-2 or knows a reliable source to obtain them, I would be extremely grateful. These files are necessary for completing my ASI network configuration correctly.

Thank you in advance for any help or advice!