Sawtooth (Customer) asked a question.
Codesys High Speed Outputs
I am evaluating using the P2CDS-622 for an upcoming project. I will need basic digital I/O, MQTT and possibly High Speed Outputs to drive ClearPath Servos. I see that the HSO modules are not currently supported. Is there a plan/path to support these and other high speed modules in the Codesys CPU?
Sorry for the late response. Currently at this time there are no plans for supporting the P2-HSO.
Ok. Thank you for the update.
Is Codesys a requirement? If not any CPU other than the P1-540 in the productivity suite should be able to do all that.
No, not a requirement, just wanting to try out the Codesys system/environment and wondering if this project would be a good fit. Fall back plan is to use the P2-622.