Rogue Fabrication (Customer) asked a question.
I am looking for a level converter for P1AM GPIO that will output 10mA
I am using the P1AM-100 GPIO to send step pulses to several different stepper and servo drives. I am using a multi-channel module (DONGKER, available through Amazon) that works with all but one of my drives -- a servo drive requiring 10mA inputs. Can someone suggest a solution that will work with this drive? It can be an optocoupler module, an SSR, or a chipset with 24V (preferred), 12V, or 5V outputs, sinking or sourcing. The maximum frequency is 4000Hz.
Note that Productivity-1000 modules including the PWM work fine with this drive.
Google 10ma stepper driver
Digital Stepper Driver 0.3-2.2A 10-30VDC for Nema 8, 11, 14, 16, 17 Stepper Motor - DM320T | StepperOnline
Thanks, but I already have the drives I need. I'm looking for a level converter (optocoupler module, SSR, or chipset) that will work with the P1AM-100 GPIO and the Huatron PR5 servo drive tequiring 10mA step pulse inputs.