Josvx (Customer) asked a question.

Hello, i need to connect some Stride Field I/O to Click Plc, but i need to supply 24 Volts to Stride Field I/O by the same ethernet cable, is this possible?

Could you help me? I have an ethernet click plc and I need to read the inputs of some machines that are 50 meters away from the control cabinet, some years ago I used stride field i/o with a click plc, but in the current case I need to supply 24 volts with the same ethernet cable because it is not possible to use additional power supplies on the machines where stride field i/o will be installed.