JB2020 (Customer) asked a question.
I am designing a system that is going to have several remote IO bases (6 remote bases) and we have been considering using the ProtosX Field IO to add more IO points. The total number of IO points I currently have is 328 discrete, but I am thinking of adding another 300 or so discrete and 16 analog.
The system currently has 15 VFDs on it, but I may need to add 11 more if we expand it like we are thinking.
How much can the P2000 handle? I cant seem to find a total IO Number anywhere in the CPU specs.
weather the hardware onboard is is more capable or not between the P3 and the P2 or if it is a programed limit for different price points I do not know.
The P3 series has always had higher communication limits than the P2. The P3 can do up to 16 remote bases with up to 4 additional racks per base with 64 bit IO cards available the IO count can get insane. The P2 as mentioned earlier has a 8 remote base limit with 32 bit IO cards available the IO count can get up there but is nowhere near the P3 limit.
I already mentioned the 32 GS drive limit for the P3 vs 16 for the P2.
As far as motion control with PS-AMC the P3 and P2 appear the same with up to 4 PS-AMC motion controllers with up to 4 axis per motion controller.