DavidChuang (Customer) asked a question.

Cannot connect to CLICK Plus with Ethernet or USB

I just unpacked a brand new Click Plus (1 slot) device and I cannot connect to the device over Ethernet or USB.

When attempting to connect via USB, I get a PTC-020 error.

When attempting to connect via Ethernet, I get a PTC-001 error

 

In the USB connection dialog, I get no ports listed

USB Connection dialogHowever, when I click on the "Detail" button, the port does show up.

USB port listBut when I double click to select it, it does not show in the main dialog.

 

When attempting to connect via Ethernet, the PLC's do show up in the scan

Ethernet connection & scan dialogI can edit the IP addresses in this dialog, but when I try to connect I get the PTC-001 error.

 

Click programming software version is 3.70

 

Has anyone else encountered this error?

Any thoughts on a resolution?

 

DC

 


  • Todd Dice (Customer)

    I would recommend using V3.6 as others have found V3.7 buggy.

  • DavidChuang (Customer)

    Does v3.60 support the C2-NRED module?

    I was under the impression that only v3.70 supported that.

     

    DC

     

  • ADC Community_04 (AutomationDirect)

    You will need v3.7 for the C2-NRED.

    I suggest running the Click software as admin and test connecting.

    Close the software and right-click on the Click software shortcut and select Run as Administrator.

  • DavidChuang (Customer)

    I did that and it did not help.

    I am using a USB Ethernet adapter so that I can leave the built-in Ethernet port configured for my corporate network.

    I will try using the built-in port.

    Though I'm not optimistic as the USB connection was unsuccessful.

    However they give different errors so maybe there's a chance.

     

    DC

    Expand Post
    • ADC_Click_PE01 (AutomationDirect)

      Are you running any Antivirus or Firewall? Also if this is a new install of v3.70 I would recommend trying to delete and reinstall. If that does not work I would suggest calling out free Tech Support so that we can get a case started.

  • DavidChuang (Customer)

    Yes to the anti-virus and firewall stuff; it's all provisioned and managed by my corporate IT beforehand.

    I have no vote in the matter.

    I also have Do-More designer v2.10 installed and that has no problems using the USB Ethernet adapter or just straight USB to connect to it's respective devices.

    And if you're wondering, I still get this issue whether the Do-More software is running or not.

     

    I'm not sure what you mean by new install of v3.70?

    I had v3.60 installed previously and installed v3.70 to work with a newly acquired Click Plus and C2-NRED

    So as far as Click software goes, no, but as far as versions go, yes.

     

    I tried the built-in network port; no luck.

    Expand Post
  • DavidChuang (Customer)

    Out of desperation, I reinstalled v3.70 and that seemed to work.

    I don't know why or how.

    Firmware update of the hardware is dodgy over Ethernet; it failed the first time.

    I reconnected via USB and that was much better.

     

    DC

     

    • ADC_Click_PE01 (AutomationDirect)

      A reinstall if v3.70 is what I meant. Glad you are now connected