McFall22 (Customer) asked a question.

PAL EIP Local Error and Digital Input Error

Hello,

 

I have a small set up with one S01, one EIP, and one B4814 with 4 V2-32C32A valves.

 

When I connect power to the module it immediately starts flashing red for Local Error and all the LEDS on the SO1 come on. When I swap the B4814 with a B4414 all the errors clear and the inputs work correctly.

 

What am I missing?

 

I also have the C2 end cap but it doesn't make a difference.


McFall22 likes this.
  • ADC Community_04 (AutomationDirect)

    Any time a hardware change is made, you should remove the access panel on the controller and press and hold the red button while powering up the unit. Continue holding until all the LEDs flash. Have you tried that?

    image

  • McFall22 (Customer)

    That did it! Thank you idk how I missed that in the manual.