Todd Dice (Customer) asked a question.
I am unable to import tags from a CM5 C-More project, originally created for an EA9 but converted to CM5 and working fine, into a PSuite project using V4.2.1.8.
I've had both projects working for a week now without issue but need to add tags into Psuite for tools in the C-more originally used on a separate project (I copied a screen from the prior project. This may be a time to write what would would be nice is allowing me - in PSuite - to add the tags and give them the addresses they were originally assigned since there will not be an address conflict, but I digress.)
Edit: I now realize I can change the assigned addresses to the tags in the C-more.
I get this warning message:
You can't directly import C-more tagDB into Productivity Suite software. This is due to the C-more tagDB export file header row is not formatted correctly to import into Productivity Suite. If you compare an C-more export file to a Productivity export file and compare the header row you will see the correct format needed.