goldminehelper (Customer) asked a question.

Easiest way to program the same input to switch between 2 different outputs every other cycle

Yes I'm new to programming a click plc. I want to have the same input switch between 2 different outputs every other cycle. I have a rotation table that requires 2 different solenoids to rotate back and forth to spin the table. So solenoid A energizes to move the table then solenoid B has to energize to spin the table. Then back to solenoid A and on and on. And if possible set up a timer to just allow like 2 seconds to each solenoid then it turns off the output.