pauljurczak (Customer) asked a question.

Is modifying an index in motion allowed on LS Electric L7PA010U-AD?

I have to execute many single motions (indexes) with positions unknown beforehand and delivered in real time. I would like to execute them as the same index 0 with different corresponding distances. Action of the index 0 is set to Stop. Can index's distance be updated (written to) while the motion is still in progress? What is the earliest time on this diagram when distance of index n1=0 can be updated:

 

Screenshot from 2024-04-20 21-51-06Do I have to use a pair of indexes, one in motion, the other one being modified, for this scheme to work?

 


  • ADC_LSElectricPLC_PE (AutomationDirect)

    XPM_DST is available to perform direct start motion. This allows you to do motion without needing to use the position table.

  • Nick234 (Customer)

    ADC, if you do mind me asking, Is there another servo drive model from LS electric that could do XPM_DST from different(non ls electric) PLC?

     

10 of 17