tech-e-80 (Customer) asked a question.
Here are the list of errors I am getting. I get these errors on two different PCs and it is only when I add the Symbol Configuration. If I build a standard project without the PS-CDS-622 package I do not get these errors...
------ Build started: Application: Device.Application -------
Typify code...
[ERROR] iecvaraccess, 4.5.0.0 (system): FB_Exit [IecVarAccess]: C0046: Identifier 'IecVarAccUnregisterInstance' not defined
[ERROR] iecvaraccess, 4.5.0.0 (system): FB_Exit [IecVarAccess]: C0035: Program name, function or function block instance expected instead of 'IecVarAccUnregisterInstance'
[ERROR] iecvaraccess, 4.5.0.0 (system): Initialize [IecVarAccess]: C0032: Cannot convert type 'Unknown type: 'IecVarAccRegisterInstance3(_IIecVarAccess3, ADR(result))'' to type 'POINTER TO BYTE'
[ERROR] iecvaraccess, 4.5.0.0 (system): Initialize [IecVarAccess]: C0046: Identifier 'IecVarAccRegisterInstance3' not defined
[ERROR] iecvaraccess, 4.5.0.0 (system): Initialize [IecVarAccess]: C0035: Program name, function or function block instance expected instead of 'IecVarAccRegisterInstance3'
Compile complete -- 5 errors, 0 warnings
Update- building a "Symbol Configuration" Object will generate errors since it is primarily targeted for OPC-UA applications (an associated Library created has OPC-UA items) and the P2CDS-622 does not support this fieldbus. The XML file is still generated though with the Tags/Variables defined in the Symbol Configuration.
We will post this on the website as "Unsupported". There is no fixed planned since OPC-UA is not offered with the P2CDS-622.