Milller6386 (Customer) asked a question.

Is there a way to force or toggle bits in Click

I am used to other software and haven't found a way to toggle or force bits. Is this possible with Click? If not what about Do more?


  • shanem717 (Customer)

    on click software, open new or current project, when open on left side of screen under the navigation menu you will see 3 menus, program/function/plc, under the program menu open monitor drop menu, then select data view, a pop up will come on screen. add the I/Os you want to overide and new on or off states then press write all new values button to send to plc, there is also check box on right side of pop up screen to view which I/Os you added are overwritten, make sure to remove all over rides before continuing normal operation of plc

    Expand Post
    Selected as Best
  • HOST_franji1 (HOST Engineering)

    For Do-more, Designer lets you Force bits (Debug->Configure Forces dialog). You can easily change the state of a bit (toggle) from Data View or Change Value dialog. Programmatically, if by Force you mean SET and RST (Reset), then YES. Also programmatically, PONOFF (Push On/Off) will toggle its output bit whenever the ladder input leg to the PONOFF box transitions from OFF to ON.

  • shanem717 (Customer)

    on click software, open new or current project, when open on left side of screen under the navigation menu you will see 3 menus, program/function/plc, under the program menu open monitor drop menu, then select data view, a pop up will come on screen. add the I/Os you want to overide and new on or off states then press write all new values button to send to plc, there is also check box on right side of pop up screen to view which I/Os you added are overwritten, make sure to remove all over rides before continuing normal operation of plc

    Expand Post
    Selected as Best
    • Milller6386 (Customer)

      This was exactly what I was looking for Thank You!!!!!!!!!