Sparkyinak (Customer) asked a question.
Is there a list flying around that lists how much memory each instruction, counter, etc. takes up in the the Click's memory? This is very handy in several ways like looking to replace another PLC with a Click knowing the count for each instruction, or estimating a program size before going down the rabbit hole just to find out (the hard way) the needs of the program exceed the controller's capacity just to name a couple. I have seen this type of information listed with some other controllers so it does not hurt to ask.
Thank you in advance
The Click plc can have a program size of 8,000 steps. The amount of steps each instruction consumes is not documented. In addition, if you want to store program documentation (rung comments, nicknames, etc.) this would contribute to the overall project file size:
https://cdn.automationdirect.com/static/specs/P1-540.pdf